MITSUBISHI ELECTRIC Changes for the Better

MELSEC MX Controller MX-F model

The MELSEC MX Controller is a series of controllers that integrates three types of control, sequence, motion, and network.
The MELSEC MX-F Controller diversified and sophisticated system can be constructed by using the MX-F models with the MELSEC iQ-F Series modules.

A first look at the controller

One controller for all your control needs

Decades of expertise in programmable controller technology have been combined into a single controller. By integrating sequence control, motion control, and network control on the MELSEC MX Controller platform, faster and more accurate control is achieved. We will continue to add functionality to this platform, making it adaptable to a wide range of applications.

Equipped with a high-performance multi-core MPU as standard, enabling high-speed control

All functions of sequence, motion, and network are integrated, achieving high-speed and high-accuracy motion control.

Details of the MX-F model

Relevant insigths - worth knowing

The MELSEC MX-F Controller can be used with MELSEC iQ-F Series products listed in the latest catalog 

System configuration example - MX-F model

*1: Future support