| Date of information | Affected Products | Summary | Detailed Information |
|---|---|---|---|
| April 2025 | Some of AC servo motors, manufactured between January 2021 and September 2024 are in target (please check detailed information for targeted products). | The primer of the components used for some of AC servo motors, manufactured and sold by our company was found to contain the phthalate ester above the maximum concentration values under RoHS2 Directive. | Technical Bulletin | Notice of EU RoHS Directive on Servomotor |
| April 2025 | Some of Three-phase squirrel-cage motors, manufactured between January 2021 and January 2025 are in target (please check detailed information for targeted products). | The primer of the components used for some of Three-phase squirrel-cage motor, manufactured and sold by our company was found to contain the phthalate ester above the maximum concentration values under RoHS2 Directive. | Technical Bulletin | Notice of EU RoHS Directive on Three-phase squirrel-cage Motor |
| November 2024 | MELSEC iQ-R series, MELSEC-Q series, MELSEC-L series, MELSEC-A series, Network products, MELIPC series | This technical bulletin informs you of compliance with substances that were added to Annex A (Elimination) of the Stockholm Convention on Persistent Organic Pollutants. | Technical Bulletin | Compliance with Substances Banned by the Stockholm Convention on Persistent Organic Pollutants |
| November 2024 | EMU4-CNT-MB EMU4-LM EMU4-BT | This technical bulletin informs you of changes about the following batteries and products with built-in batteries to comply with the regulations | Technical Bulletin | Compliance with EU Battery Regulations for Power Management Meters and Energy Saving Supporting Devices |
| November 2024 | Q8BAT,Q8Bat-SET | This technical bulletin informs you of changes about the following batteries and products with built-in batteries to comply with the regulations | Technical Bulletin | Compliance with EU Battery Regulations for MELSEC series, MELIPC series, and GOT2000 series |
| November 2024 | IU2-BATT FX3U-32BL | This technical bulletin informs you of the change in the MELQIC series batteries. | Technical Bulletin | Compliance with EU Battery Regulations for MELQIC series |
| November 2024 | MR-BAT6V1SET(- ) , MR-BAT6V1, MR-BAT6V1BJ, MR-BAT, MR-J3BAT, MR-J3W03BATSET, MR-J2M-BT(- ) , MR-JBAT4, and MR-JBAT8 | For battery products for the AC servo amplifiers, built-in batteries will bear the CE mark to comply with the requirements of the EU Battery Regulation (REGULATION (EU) 2023/1542) | Technical Bulletin | Adding CE Mark on Batteries for AC Servo Amplifiers in Compliance with EU Battery Regulation |
| November 2024 | Model with built-in battery:Q172DEX, Q172DSCPU, Q173DSCPU, Q172DCPU, Q173DCPU, Q170MSCPU, Q170MCPU, MR-MQ100, Q170MSBATN-SET, Q170MBATN-SET | The battery label will be changed as follows to comply with the EU Battery Regulation. | Technical Bulletin | Battery Label Change in Compliance with EU Battery Regulation |
| November 2024 | MELSEC iQ-F Series, MELSEC-F Series, network products | Compliance with Substances Banned by Stockholm Convention on Persistent Organic Pollutants, Dechlorane Plus and UV-238 | Technical Bulletin | Compliance with Substances Banned by Stockholm Convention on Persistent Organic Pollutants |
| January 2023 | General | Our FA products will be implemented marking that complies with the European WEEE Directive. See the linked document. Please note that regardless of whether this symbol is marked on the product or not, at their end-of-life, please contact a certified electronic waste disposal company for the environmentally safe recycling and disposal of your device, separately from your household waste. | Our Compliance with WEEE Directive |
| Date of information | Affected Products | Vulnerability | Countermeasure | Detailed Information |
|---|---|---|---|---|
| 04.04.2025 | Mitsubishi Electric Europe B.V. smartRTU version 3.37 and prior | CVE-2025-3128, CVE-2025-3232 | Please refer to the vulnerability report under Detailed Information | MEU_PSIRT_2025-3128 |
| 01.04.2023 | ME-RTU | CISA-23-110-01 CVE-2023-2131 | Issue has been solved with Firmware v3.36. Additional improvements will be done with v3.37 | - |
| 01.10.2021 | ME-RTU | CVE-2018-16060 | Issue has been solved with Firmware v3.35 | - |
| 01.09.2019 | ME-RTU | ICS-ALERT-19-225-01 | Issue has been solved with Firmware v3.36. Additional improvements will be done with v3.37 | - |
| 01.08.2019 | ME-RTU | CVE-2019-14930 | Issue has been solved with Firmware v3.36. Additional improvement with v3.37 for redundant users | - |